Status - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
Note: The value of the Status attribute displays next to the Default Attribute for Display (typically Present Value) in the header bar of the Display panel.

Displays the highest priority Status for the object.

Examples: (in order of priority - supported states depend on Object Type)

  • Out Of Service: The Out Of Service attribute value is True.

  • Offline: Communication with the physical hardware has failed.

  • Unreliable: Reliability attribute is not reliable.

  • Alarm: Object or alarm extension has an alarm state.

  • Normal: No abnormal condition for this object detected.

Back to Common Attributes.