Common Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
This section lists the attributes that are common to BCPro system objects. Click the attribute name in the table for a description of the attribute.

For detailed information on BACnet properties, refer to ANSI/ASHRAE Standard 135-2008 - A Data Communication Protocol for Building Automation and Control Networks.

Table 1. Common Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Archive Date

Date

       

Alarm State

One state from a set

   

Normal

Subset of the Object Status (Set 505)

Description

Text

CNW

BNW

No text

Maximum 40 characters

Enabled

True or False

   

True

 

Item Reference

Text

C

   

All Items navigation tree path to object. SiteID:DeviceID/x.y.z

Name

Text

CW

 

Item ID

Maximum 400 characters (40 or less is best for display layout)

During online creation, this field is limited to 32 characters; however, you can edit and lengthen the name later.

Object Category

One type from a set

CW

W

General

HVAC, Fire, Security, Services, Administrative, General, Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System, Custom 1–12

Object Count

Number

       

Object Identifier

Number

C

B

 

Instance Number of Object Type within the host device

Object Name

Text

 

B

 

Item Reference less SiteID

Object Type

One type from a set

 

B

 

Actual Object Type

Status

One state from a set

   

Normal

(Displayed in panel header.)

Version

       

Actual version of Object in device

1 B - Exposed as Standard BACnet Property, C - Configurable, N - Value Not Required, W - Writable