Commanding an Item - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

About this task

Note: You must be in online mode to issue commands to items.

To command an item:

Procedure

  1. Select the item to command in the navigation tree or in the display panel.
  2. From the Action Menu, select Commands, or right-click and select Commands.
  3. Filter the list of commands using the Show Command Set drop-down menu, if desired.
  4. Select the command to issue.
    Note: After selecting one of the available commands, you may be prompted to specify additional parameters for the command.
  5. Click Send.
    Note: If an error occurs while sending the command, the dialog box remains open.