Calendar Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Calendar Attributes - Calendar Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Date List (Entry Detail)

Date/Time

CW

W

   

Global Calendar Object Reference

Attribute reference

CW

W

   

Global Calendar Update

Date/Time

       

Present Value

True or False

D

D

False

 
1 C - Configurable, D - Default Attribute for Display, W - Writable