Status Flags - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Contains four true or false flags that indicate the general health of the object. Three of the four flags are associated with the values of other attributes within the same object. By reading these attributes, you can achieve a clearer picture of the object status.

The four flags are:
  • In Alarm - In Alarm flag is False (0) if the Event State attribute value is Normal; otherwise, the In Alarm flag is True (1).
  • Fault - Fault flag is True (1) if the Reliability attribute is not reliable; otherwise, the Fault flag is False (0).
  • Overridden - Overridden flag is Logical 1 if the Present Value has been overridden by some mechanism local to the BACnet device or because operator intervention provided a different value.
  • Out of Service - Out of Service flag is True if the Out of Service attribute value is True; otherwise, the Out of Service flag is False.

Back to Binary Value Attributes.