Binary Value Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Binary Value Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Active Text 2

Text

     

Limit: 20 characters

Active Time Reset

Date/Time

       

COS Count 3

Number

W

 

0

0–4,294,967,295

COS Time 3

Date/Time

   

Null

 

Elapsed Active Time 4

Number

   

Null

0–4,294,967,295

Units = seconds

Inactive Text 2

Text

     

Limit: 20 characters

Min Off Time

Number

CW

W

0

0–4,294,967,295

Units = seconds

Min On Time

Number

CW

W

0

0–4,294,967,295

Units = seconds

Out of Service

True or False

 

W

False

Always False

Present Value 5

Multistate

DRW

DRW

 

Inactive, Active States Text attribute identifies the value set for this attribute.

Priority Array

Set of values

       

Reliability

Multistate

W

W

Reliable

No Fault Detected (Reliable), Unreliable Other, Communication Failure

State Count Reset 3

Date/Time

       

States Text

One state from a set

CW

 

Inactive, Active

 

Status Flags

Series of True or False states

     

In Alarm, Fault, Overridden, Out of Service

1 C - Configurable, D - Default Attribute for Display, R - Affected by Object’s Reliability, W - Writable
2 If either Inactive Text or Active Text is present, both are present.
3 If Change of State Time, Change of State Count, or State Count Reset is present, all are present.
4 If either Elapsed Active Time or Active Time Reset is present, both are present.
5 Present Value is commandable; it is also writable. This attribute is writable when Out of Service is True.