Binary Value Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Binary Value objects have similar software characteristics and capabilities to a Binary Input Object; however, Binary Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold a binary value for other objects to reference. For example, an Interlock Object can reference and base its operation on a binary value such as duty/standby.

For general information on BCPro system objects, see Common Object Attributes.