Binary Output Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. Binary Output Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Active Text

Text

     

Limit: 20 characters

Active Time Reset

Date/Time

       

COS Count

Number

W

 

0

0–4,294,967,295

COS Time

Date/Time

       

Device Type

Text

CW

W

Null

Limit: 20 characters

Elapsed Active Time

Number

   

0

0–4,294,967,295

Units = seconds

Heavy Equip Delay

Number

CW

Not supported

0

Range: 0–255 Seconds

HED Controller

Number

CW

Not supported

 

1–5

Inactive Text

Text

     

Limit: 20 characters

Min Off Time

Number

CW

W

0

0–604,800

Units = seconds

Min On Time

Number

CW

W

0

0–604,800

Units = seconds

Out of Service

True or False

 

W

 

False

True

Polarity

One value from a set

     

Normal, Reverse

Present Value

One value from a set

DRW

DRW

 

Inactive, Active States Text attribute identifies the value set for this attribute.

Priority Array

Set of values

       

Reliability

One value from a set

   

Reliable

No Fault Detected (Reliable), No Output, Open Loop, Shorted Loop, Unreliable Other, Communication Failure

State Count Reset

Date/Time

       

States Text

One value from a set

CW

 

Off

On

 

Status Flag

Series of True or False states

   

False,

False,

False,

False

In Alarm, Fault, Overridden, Out of Service

1 C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object’s Reliability, W - Writable