Binary Output Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English
The BO object’s attributes represent the external, visible characteristics of a binary output. As a binary output, this object can be in either an Active or Inactive state. The Polarity attribute allows for normally open relays that are Active when energized and normally closed relays that are Inactive when energized. This object integrates BACnet controllers into supervisory controllers, resulting in:
  • a consistent interface to point objects for all controller types, so they appear as a homogenous set to the user interface
  • flexibility in point mapping
  • support for all BCPro system controllers.

For example, this object allows you to start or stop a fan from a supervisory controller.

For general information on BCPro system objects, see Common Object Attributes.