Reliability - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Examples:
  • Reliable - No detectable faults
  • Communication Failure - Communication to the sensor or device reading the sensor has failed.

When Out of Service is True, the Reliability attribute may be written directly.

Back to Binary Input Attributes.