Characterizes the intended effect of the Inactive state of Present Value attribute from the viewpoint of the operator. The content of this string is a local matter, but it is intended to represent a readable description of the Inactive state.
For example, if the physical input is connected to a switch contact, then the Inactive Text attribute is assigned a value such as Fan 1 Off. If either the Inactive Text or Active Text attribute is present, both are present.
Back to Binary Input Attributes.