Binary Input Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. Binary Input Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

BACnet Notes1

Initial Value

Values/Options/Range

Active Text 2

Text

 

B

 

Limit: 20 characters

Active Time Reset 3

Date/Time

 

B

   

COS Count 4

Number

W

B

 

0–4,294,967,295

COS Time 4

Date/Time

 

B

   

Device Type

Text

CW

BW

Null

Limit: 20 characters

Elapsed Active time

Number

 

B

Null

0–4,294,967,295

Units = seconds

Inactive Text 2

Text

 

B

 

Limit: 20 characters

Out of Service

True or False

CW

BW

False

 

Polarity

One value from a set

 

BW

 

Normal, Reverse

Present Value

Real value

DNRW

BW

0

 

Reliability

One state from a set

W

BW

Reliable

No Fault Detected (Reliable), No Sensor, Open Loop, Shorted Loop, Unreliable Other, Communication Failure

State Count Reset 4

Date/Time

 

B

   

States Text

One value from a list

CW

 

Off

On

 

Status Flags

Series of True or False values

 

B

False,

False,

False,

False

In Alarm, Fault, Overridden, Out of Service

1 B - Exposed as Standard BACnet Property, C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object Reliability, W - Writable
2 If either Inactive Text or Active Text is present, both are present.
3 If either Elapsed Active Time or Time of Active Time Reset is present, both are present.
4 If Change of State Time, Change of State Count, or Time of State Count Reset is present, all are present.