Binary Input Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
The BI object’s attributes represent the external, visible characteristics of a binary input. As a binary input, this object can be in either an Active or Inactive state. The Polarity attribute allows for normally open relays that are Active when energized and normally closed relays that are Inactive when energized.
The Binary Input object integrates BACnet controllers into supervisory controllers, resulting in:
  • a consistent interface to point objects for all controller types, so they appear as a homogenous set to the user interface
  • flexibility in point mapping
  • support for all BCPro system controllers.

For example, this object allows you to map a fan status into a supervisory controller.

For general information on BCPro system objects, see Common Object Attributes.