Status Bar Icon - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Icons in the Status bar indicate system activity (Table 1).
Table 1. Status Bar Icons/Text

Icon/Text

Description

This icon appears if the BCPro Data Server software is sending or receiving view data to or from the BCPro Workstation and network devices.

This icon appears when diagnostic information for the BCPro Data Server user interface is available. If you click this icon, the User Interface Diagnostics window appears.

Time Zone/ Date/Time

The status bar of the BCPro UI displays the date, time, and time zone of the device to which you are logged-in. Due to the time it takes to retrieve the time from the device, the status bar time may lag slightly behind the device’s actual time. If the device reports an unsupported time zone, the BCPro UI defaults to UTC.