Screen Layout and Frames - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

The screen contains four frames and provides a consistent look and feel in every mode (online or offline). Your access to certain features depends on the mode in which you are operating and your assigned access type and privileges.

Note: If the navigation frame or a display frame is active, the header bar of the active frame or pane is highlighted. The Menu and Status frames are not highlighted even when you click in them.
Figure 1. Basic Screen Layout

Table 1. BCPro Data Server UI Screen Frames

Number

Name

Description

1

Menu

Displays the menu bar.

For more information on menus, see Pop-up Menus. Log out or exit from the system using buttons in the menu frame.

2

Display

Presents data or information in the user-selected panel layout. In the preceding example, the Display Frame contains two Display Panels. The top Display Panel shows information about the BCPro Workstation (the device is selected in the navigation tree and the name of the device appears at the top of the Display Panel). The bottom Display Panel contains a summary of the points monitored by a field device. See the Display Frame section for more information.

3

Navigation

Displays navigation trees that organize items in the system. The All Items tree generates automatically when you configure the system database. You can create one or several folders for defining your own navigation concept.

For more information on the navigation tree, see the Navigation Tree section.

4

Date/Time

Displays the current date, time, and time zone of the BCPro server that you are logged into.