Pop-up Menus - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Pop-up menus provide an efficient way to quickly access important item information. Pop-up menus are also referred to as right-click menus. To access pop-up menus, right-click an item in the navigation tree. Content of the menu depends on the type of selected item and your level of authorization. For example, point object pop-up menus usually show the options View, Command, and Show Extensions. For devices, pop-ups usually show View, Command, Modify, and Show Extensions.