Display Panel Tabs - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Each display panel contains tabs that vary depending on the item displayed.

For example, most of the point objects, such as the OAT contain the following tabs:
Table 1. Tabs

Tab

Description

Focus

Becomes available when you define a point object. The Focus tab shows operation attributes available for the object type to which the object belongs. Please note that the Basic and Advanced radio buttons allow you to filter the attribute display in this tab. The Edit button allows you to change configurable attributes.

Hardware

Becomes available when you define a point object that has a reference to a physical input or output. The Hardware tab shows hardware-related attributes available for the object type to which the point object belongs.

Trend

Becomes available when you create a Trend Extension for an object (see Trend Extensions). New and Delete buttons allow you to add or delete Trend Extensions for the point. The Chart view allows you to view data samples in a graphical format and retrieve new trend data. The Table view of the Trend Extension allows you to view the trend’s data samples in a table format. The Definition view of the Trend Extension allows you to view and edit the attributes of the trend extension object.

Note: In the BCPro Data Server, the Trend extension is only available to Router and Gateway device objects.
Other items may contain fewer or more tabs. For example, the item representing the Workstation or Router contains the following tabs:
  • Focus
  • Summary
  • Diagnostic
  • Engineering
  • Network
  • Trend

For information on the tabs available in the system, see the Object and Feature Tabs section.