Commands - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Use commands to force an item to perform a specific action. For example, ON and OFF commands for a binary output make a fan run or stop, and the Reset Device command for a Router or Gateway.

For information on which commands an item supports, see the appropriate topic in the Object Help.

For information on how to send a command, see Commanding an Item in the Commands Dialog Box section.