Online Mode - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

When you are connected to the BCPro Workstation, you can perform online operational activities such as monitoring and commanding equipment. You can also perform online database configuration activities, such as defining field controllers or adding points. This function is referred to as online mode or online Site BCPro UI. The online mode is available to users with the Access Type of Standard Access or Basic Access. See the Access Types section.

Any changes you make to the system configuration are made online to the system and need to be uploaded to be stored in the archive database.