Offline Mode - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

BCT is a standalone software program installed on your computer, including the BCPRo Server, that allows you to configure the BCPro Servers, Routers, and Gateways without being connected to the live BCPro Data Server server and devices; this function is called the offline mode. In offline (system configuration) mode, use BCT to set up the system database. You must load configuration changes created in offline mode to the Routers and Gateways for the settings to take effect. See Database Uploading, Downloading, Upgrading Device and Synchronization.

These features are available only with BCT: ActionQ and Database Uploading, Downloading, Upgrading Device and Synchronization. You can only add servers, Routers, and Gateways in offline mode.

The offline mode is available to users with the Access Type of Standard Access. See the Access Types section.