BCPro Data Server can operate in two different modes: online using the BCPro UI or offline using the BCT. When you are connected to the BCPro Workstation, you can perform online mode operational activities such as monitoring and commanding. When you are connected to the BCT only, you can perform offline mode system configuration tasks such as configuring point objects and features.