BCPro Data Server User Interface - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

You can interact with the entire BCPro Data Server from any location running a supported web browser. Windows® Internet Explorer® version 9.0 or 10.0 is recommended. Other browsers, such as Apple® Safari®, Mozilla Firefox, or Google® Chrome may also be used but are not fully supported. After you log in to the BCPro Data Server, you are able to perform the following operations:

For more information on the specific features of your BCPro Data Server, see the features listed in the table of contents in this Help file. For more information on menus, see Menus.