Local Abort Tx - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains the number of application layer abort messages generated locally (for example, messages that used up all allowed retries and did not get an acknowledge from the remote device).

Back to BACnet Protocol Engine Attributes.