BACnet Protocol Engine Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. BACnet Protocol Engine Attributes - Diagnostic Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Abort Rcv

Number

 

0

 

Abort Tx

Number

 

0

 

Ack Rcv

Number

 

0

 

Ack Tx

Number

 

0

 

Allocated Record Count

Number

 

0

 

Clear Statistics

True or False

 

False

 

Conf Req Rcv

Number

 

0

 

Conf Req Tx

Number

 

0

 

Error Rcv

Number

 

0

 

Error Tx

Number

 

0

 

Latch Statistics

True or False

 

False

 

Local Abort Tx

Number

 

0

 

Net Messages Rcv

Number

 

0

 

Net Message Tx

Number

 

0

 

Net Rejects Rcv

Number

 

0

 

Net Routed Messages

Number

 

0

 

Net Routes Busy

Number

 

0

 

Net Unknown Msg Rcv

Number

 

0

 

Net Unknown Routes

Number

 

0

 

Peak Pending Queue Count

Number

 

0

 

Peak Unknown Queue Count

Number

 

0

 

Pending Queue Count

Number

 

0

 

Rcv Messages Discarded

Number

 

0

 

Rcv Msg Rate

Number

 

0

 

Rcv Record Count

Number

 

0

 

Record Count

Number

 

0

 

Reject Rcv

Number

 

0

 

Reject Tx

Number

 

0

 

Req Retries Tx

Number

 

0

 

Reset Date

Date

     

Reset Time

Time

     

Seg Ack Rcv

Number

 

0

 

Segment Ack Tx

Number

 

0

 

Seg Conf Req Rcv

Number

 

0

 

Seg Conf Req Tx

Number

 

0

 

Seg Retries Tx

Number

 

0

 

Segment Ack Rcv

Number

 

0

 

Segment Ack Tx

Number

 

0

 

Segment Rcv

Number

 

0

 

Segment Tx

Number

 

0

 

Simple Ack Rcv

Number

 

0

 

Simple Ack Tx

Number

 

0

 

Transaction Timeouts

Number

 

0

 

Transmits Per Minutes

Number

 

0

 

Tx Messages Discarded

Number

 

0

 

Tx Record Count

Number

 

0

 

Unconfirmed Rcv

Number

 

0

 

Unconfirmed Tx

Number

 

0

 

Unknown Queue Count

Number

 

0

 
1 C - Configurable, N - Value Not Required, W - Writable