Polled Object Count - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the number of mapped BACnet objects currently being polled on a periodic basis. The polling is limited to those mapped BACnet objects which are currently being accessed either by a feature or the UI (the Instance Number is typically smaller than the total Count).

Back to BACnet Integration Attributes.