Execution Time - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Records the amount of time taken for the last periodic update of all integrated BACnet objects. The value for this attribute can be used to tune the Periodic Update attribute. If the Execution Time is greater than the Periodic Update, attribute values of integrated BACnet objects are constantly being updated over the network.

Back to BACnet Integration Attributes.