Duplicate Device Identifiers - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Lists any duplicate BACnet Device Object Identifiers found after an auto-discovery of BACnet devices is performed. The list contains the instance number of the BACnet Device Object Identifier and the network address (represented in hex notation) of each device with the same identifier instance number as another device on the network. The devices in this list are not included in the list of auto-discovered devices in the integration tree under the Engineering tab of the BACnet Integration object. The physical locations of BACnet devices with duplicate device identifiers must be determined, and their object identifiers changed to make them unique network-wide.

Back to BACnet Integration Attributes.