BACnet Integration Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.
Table 1. BACnet Integration Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes 1

Initial Value

Values/Options/Range

Count

Number

     

Device Discovery Range

Structure

CW

 

Structure elements:

  • network number (see attribute description)
  • high limit device instance (Range: 1–4,194,302)
  • low limit device instance (Range: 1–4,194,302)

Periodic Update

Number

CW

60

0–65,535

Units = seconds

Poll Delay

Number

CW

 

Milliseconds

10–50

Preserve Discovered Devices

True or False

CW

True

 

Requested Vendor ID

Number

CNW

 

0–65,535

The current list of Vendor IDs can be viewed at http://www.bacnet.org/VendorID/BACnet%20Vendor%20IDs.htm.

Table 2. BACnet Integration Attributes - Diagnostic Tab

Attribute Name

Data Type

Notes 2

Initial Value

Values/Options/Range

Duplicate Device Identifiers

List

     

Execution Time

Number

   

0–4,294,967,295

Units = seconds

Polled Object Count

Number

     
1 C - Configurable, N - Value Not Required, W - Writable
2 C - Configurable, N - Value Not Required, W - Writable