BACnet Integration Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The BACnet Integration object manages the communication with a BACnet network. All integrated BACnet devices and objects appear under the BACnet Integration object in the Navigation Tree.

The BACnet Integration object serves as the root for all integrated BACnet objects on an Ethernet trunk. The BACnet Integration object is a direct child of a supervisory controller and integrates BACnet devices using the Ethernet trunk.

For general information on BCPro system objects, see the Objects section.

For detailed information on the BACnet Integration object, see BACnet Integration Attributes.