VT Classes Supported - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains a list of BACnet Video Terminal (VT) Classes that indicate a particular set of terminal characteristics. A device often supports multiple types of behaviors for differing types of terminals or differing types of operator interface programs. If either VT Classes Supported or Active VT Sessions is present, then both are present. Both are required if support of VT Services is indicated in the PICS.

Back to BACnet Device Attributes.