Time Sync Recipients - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Controls the restrictions placed on a device’s use of the Time Synchronization service. If the list is of length zero, a device is prohibited from automatically sending a Time Synchronization request. If the list is of length one or more, a device automatically sends a Time Synchronization request but only to the devices or addresses listed. If it is present, this attribute is writable. If the PICS indicates that this device is a Time Master, then Time Synchronization Recipients is present.

Back to BACnet Device Attributes.