Indicates the minor revision level of the BACnet standard. This starts at 1 and increases for each subsequent release. If the Protocol Version attribute changes, this number reverts to zero. This attribute is required for all devices with BACnet Protocol Version 1, Protocol Revision 1 and above. If this attribute is not present, the device is Protocol Version 1, Protocol Revision 0.
Back to BACnet Device Attributes.