Protocol Obj Support - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates which standardized object types the device’s protocol implementation supports. This attribute reflects the minimum set of object types, but implementation often supports additional standard and non-standard object types with their own set of attributes. (The list of attributes supported for a particular object may be acquired by use of the Read Property Multiple service with an attribute reference of All.)

Back to BACnet Device Attributes.