Profile Name - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains a string of characters that represents the name of the object profile to which the object conforms. A profile name must begin with a vendor identifier code in base-10 integer format, followed by a dash. The vendor identifier code indicates the organization that administers the remaining characters of the profile name, and publishes and maintains the profile document identified by the profile name. The vendor identifier does not need to match the vendor identifier of the device in which the object resides.

Back to BACnet Device Attributes.