Specifies the highest possible address for master nodes and is less than or equal to 127. This is present if the device is a master node on an MS/TP network. If Max Master is not writable via BACnet services, its value is 127.
Back to BACnet Device Attributes.