Contains a list of BACnet Object Identifiers of a BACnet Device object and a BACnet device address in the form of a BACnet Address. Entries in the list identify the actual device addresses that are used when accessing the remote device via a BACnet service request. The list may be empty if no device identifier-device address bindings are currently known to the device.
Back to BACnet Device Attributes.