Active VT Sessions - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Specifies a list containing a Local Video Terminal (VT) Session Identifier, a Remote VT Session Identifier, and Remote VT Address. This attribute provides a network-visible indication of those VT sessions that are active. When a VT session is created with the VT-Open service, a new entry is added to the Active VT Sessions list. When a VT session terminates, the corresponding entry is removed from the Active VT Sessions list. If either VT Classes Supported or Active VT Sessions is present, then both are present. Both are required if support of VT Services is indicated in the PICS.

Back to BACnet Device Attributes.