Active COV Subscriptions - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Contains a list of BACnetCOV Subscriptions, each of which consists of a Recipient, a Monitored Property Reference, an Issue Confirmed Notifications flag, a Time Remaining value, and an optional COV Increment. This attribute provides a network-visible indication of those COV subscriptions active at any given time. Whenever a COV Subscription is created with the Subscribe COV or Subscribe COV Property service, a new entry is added to the Active COV Subscriptions list. Similarly, whenever a COV Subscription is terminated, the corresponding entry is removed from the Active COV Subscriptions list.

Back to BACnet Device Attributes.