APDU Retries - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Indicates the maximum number of times that an Application Protocol Data Unit (APDU) is retransmitted. The default value is 3. If this device does not perform retries, then this attribute is zero. If the value of this attribute is greater than zero, a nonzero value is placed in the Device object APDU Timeout attribute.

Back to BACnet Device Attributes.