BACnet Device Attributes - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

This object contains attributes common to many BCPro system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Table 1. BACnet Device Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Flags 1

Initial Value

Values/Options/Range

Align Intervals

True or False

W

False

 

APDU Retries

Number

W

3

 

APDU Timeout 2

Number

W

4,000

 

APDU Timeout

Number

 

See next column

The default is 6,000 milliseconds for devices that permit modification of this attribute. The default value is 60,000 milliseconds for all other devices.

Active COV Subscriptions 3

List

     

Active VT Sessions 4

List

     

Appl SW Version

Text

     

Backup Fail Timeout 5

Number

W

120

Units = Seconds

Configuration Files 6

Set of values

     

DST Status

True or False

W

 

True, False

Database Revision

Number

     

Description

Text

W

 

Unrestricted range

Device Addr Binding

List

W

   

Firmware Version

Text

     

Graphic

Object reference

CW

   

Graphic Alias

Text

CW

 

Maximum 256 characters

Interval Offset

Number

CW

0

Units = Minutes

Last Restore Time 6

One value from a set

     

List of Session Keys

List

     

Local Date

Date

W

   

Local Time

Time

W

   

Location

Text

W

   

Max APDU Length

Number

   

Greater or equal to 50

Max Info Frames 7

Number

 

10 (FEC)

20 (NxE)

 

Max Master 7

Number

 

127

 

Max Segments Accepted

Number

     

Model Name

Text

     

Offline

True or False

 

False

 

Profile Name

Text

     

Protocol Obj Support

Series of True or False values

     

Protocol Revision

Number

     

Protocol Ser Support

Series of True or False values

     

Protocol Version

Number

     

Restart Notification Recipients

Structure

CW

   

Segmentation

One type from a set

   

Segmented Both,

Segmented Transmit,

Segmented Receive,

No Segmentation

System Status

One type from a set

D

 

Operational, Operational Read Only, Download Required, Download in Progress, Nonoperational, Backup in Progress

Time Synchronization Interval

Number

CW

0

Units = Minutes

Time Sync Recipients 8

List

W

 

Zero or more

UTC Offset

Number

W

 

-720 though +720

VT Classes Supported 4

List

     

Vendor ID

Number

     

Vendor Name

Text

     
1 C - Configurable, D - Default Attribute for Display, W - Writable
2 If segmentation of any kind is supported, this is required.
3 If the device supports execution of either the Subscribe COV or Subscribe COV Property service, this attribute is required.
4 If either Video Terminal (VT) Classes Supported or Active VT Sessions is present, both are present. If the Protocol Implementation Conformance Statement (PICS) indicates support for VT Services, both of these attributes are present.
5 If the device supports the backup and restore procedures, this attribute must be present and writable.
6 If the device supports the backup and restore procedures, these attributes are required.
7 If the device is an MS/TP master node, these attributes are required.
8 If PICS indicates the device is a Time Master, this is required. If present, this attribute is writable.