BACnet Device Object - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Note: The Object Type for this object is labeled Non-FEC BACnet Device in the software.

The BACnet Device object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one Device object exists in each BACnet Device.

For general information on BCPro system objects, see the Objects section.

For detailed information on the BACnet Device object, see BACnet Device Attributes.