Clearing the Audit Repository - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Procedure

  1. Launch the Audit Viewer by selecting the BCPro Workstation or a device from the Device Selection Dialog box.
  2. Click anywhere in the Audit Viewer.
  3. Click Clear. All audit messages stored in that Audit Repository are cleared.
    Note: If you want to permanently store audit messages, click the Forward Messages button before clicking Clear.