Default Destination and Message Forwarding - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Default Destination defines where audit messages are sent when a user clicks the Forward Messages button in the Audit Viewer. By default, the BCPro Workstation is the Default Destination that permanently stores audit messages from the Router and Gateway devices.

You can forward audit messages to the BCPro Workstation from the Device local audit repository by clicking the Forward Messages button in the Audit Viewer. See Forwarding Audit Messages to the Default Destination.

When the Device local audit repository is 100% full, the local audit repository replaces the oldest messages (rollover) with new messages.