Audited events are significant events occurring in the system that trigger the Audit Trail feature to generate an audit message. The following table lists the features and corresponding actions that initiate the generation of audit messages. The following table also lists Audit Classes (Set 568) in which the actions belong. Click the feature name for more information about that feature.
|
Feature |
Action Causing Audit Message |
|---|---|
|
each command issued, enabled, disabled, or deleted (Audit Class = User Action) |
|
|
|
|
each errorlog listing problems with your BCPro system such as detected software or configuration errors (Audit Class = Diagnostic) |
|
|
|
|
|
|
System Security |
|
|
Navigation Tree and Other Features |
|