Audit Trail Overview - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Audit Trail feature initiates an audit message when the system detects an audited event such as a user logging on or logging off of the BCPro system, commanding an item, or changing the configuration of a device. An audit message is stored in the Audit Repositories of the device that generated the audit message. When the local audit repository is full, you can send its audit messages to a BCPro Workstation repository defined as the Default Destination for permanent storage.

The Audit Viewer allows you to view audit messages stored in the audit repository of the selected device. You can determine how to sort and filter the audit messages that appear in the Audit Viewer as well as forward them to the defined default destination. You can add annotations to audit messages and view them when displayed on a BCPro Workstation. You can also define customized annotations and add these custom annotations to audit messages.

Audit Message and Audit Viewer shows the flow of audit messages through the BCPro system.

Figure 1. Audit Message Process