Audit Trail - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

The Audit Trail feature generates audit messages and stores them in Audit Repositories. An audit message contains information about a significant event on the Building Control Management system. For audit purposes, a significant event is an action or occurrence on the system that should be recorded for later analysis of building operations. A new audit message is generated for each significant event on the BCPro system. The Audit Viewer displays the audit messages stored in an audit repository. You can access the Audit Viewer from the View Menu of the BCPro user interface in online mode.

The Audit Trail provides a historical record of the audited events, such as creating or deleting items, that have occurred within the system. By viewing audit messages, you can examine and analyze the actions that occurred in the system.