Operator Override - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Updates the Present Value at Command Priority Operator Override (8).

The Operator Override command sends the specified command to the internal NxE object, which is then only sent to the field device when not Out Of Service.

Back to Analog Value Commands.