Status Flags - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Product
Building Automation Systems > Databases and Data Servers > BCPro Data Server
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27

Indicates the general status of the Analog Input object in BACnet terms and contains four independent states.

The four flags are:
  • In Alarm - False if the Event State attribute value is Normal; otherwise, the In Alarm flag is True. (Set only by BACnet Intrinsic Alarming.)
  • Fault - True (1) if the Reliability attribute is not reliable; otherwise, the Fault flag is False.
  • Overridden - Overridden flag is True if the Present Value is overridden at the hardware source level.
  • Out of Service - Out of Service flag is True if the Out of Service attribute value is True; otherwise, the Out of Service flag is False.

Back to Analog Value Attributes.