Indicates the current value of the analog value. Present Value is optionally commandable. The optional Priority Array must be present for Present Value to be commandable. Values written to Present Value are compared with the Min Value and Max Value attributes and set the Reliability.
Back to Analog Value Attributes.