Max Value - BCPro - LIT-12011905 - Server - BCPro Data Server - 4.0

BCPro Data Server

Brand
BCPro
Product name
BCPro Data Server
Document type
User Guide
Document number
LIT-12011905
Version
4.0
Revision date
2020-03-27
Language
English

Defines the highest reliable value (in engineering units) for the Present Value.

This value is not writable for Analog Value objects in the FEC.

This value is writable if the AV is the ZN-SP on a Net Sensor. This method is the only way to set the range for the Net Sensor.

Back to Analog Value Attributes.